Other Parts Discussed in Thread: LM51561H, LM5156H, LM5156H-Q1
Hi Team,
My customer is using LM51561H-Q1 for refrigerator project.
Please review the schematic.
Input : Battery 10.5V~16V(Max 32V)
Output : 12V, 3A↓
LM51561H-Q1 schematic_20210630.pdf
Question : LM51561H, LM51561H-Q1
The customer wants to use 2 parts due to the delivery date issue.
Can I use LM51561H at the same time without modification in the schematic?