Hi team,
Could you give me comment on following customer questions?
Q1. Could you share equation how to calculate Rcomp, Ccomp, CHF in dual phase single output case? Eq. (43), (44), (45) looks dual output case, but it looks different from dual phase single output case based on the result of the quick start calculation sheet.
Q2. Based on the quick start calculation tool, the customer understands minimum Cout requirement is as follows. Is it correct understanding?
Dual phase single output: Cout1: 11uF, Cout: 11uF
Dual output: Cout1: 22uF, Cout2: 22uF
Q3. For minimum input capacitance requirement, the customer calculates Cin = 7.8uF based on the datasheet equation at dual output. Taking DC bias and the # of channels, Cin = 40uF [=(10uF x 2) x 2ch] is required. Is it the same requirement for dual phase single output? Or the minimum input capacitance requirement is a half of the dual output case of the Cin?
Best regards,
Takeshi Sasaki