This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello
If the output of the regulator is shorted, the device will protect itself, assuming the inductor does not saturate.
The best way to prevent the inductor from saturating is to choose an inductor that is rated for the current limit of the
device. In this case about 4A.
There is no way to ensure that either damage to the regulator and/or the load can be avoided with a saturated inductor.
A saturated inductor allows very high di/dt such that the current limit of the device may not be fast enough to react and
shut off the switching.
This is true of any regulator, not just this particular device.
Thanks
Hi,
Thanks for your feedback. If load is shorted, the device will enter into safe state. Understood.
I have selected the inductor with max current rating of 3.5A.
My question was regarding Failure mode effects diagnostics analysis(FMEDA), wherein if the external connected power inductor gets short(due to electrical overstress or any other phenomenon..), what would be the behavior of the buck convertor and does it goes to safe state?
Please provide your feedback.
Thanks
Hello
If the inductor is shorted, then the SW node would be connected directly to the output capacitors, and large currents would
flow through the device. Under those conditions the current limit and/or thermal shutdown may not be able to protect the
device. There is a strong likelihood that the device would be damaged. Also, the output voltage would not remain in
regulation under those conditions.
Thanks