Part Number: LM350-N
Other Parts Discussed in Thread: LM350A, LM1085
Hello TI experts,
My customer considers LM350 for their new product, instead of DCDC buck converter.
The application is medical equipment, so they are very sensitive to switching noise based on DCDC converter, and now considers LDO.
here are my few questions ;
1. what is the difference between LM350-N and LM350A? in datasheet I can see LM350A has strong points for output voltage tolerance, line regulation, load regulation.
also I see that LM350A is rated for -40 degree to +125 degree. is there more difference except I mentioned?
2. I see the Lead Temperature (metal package, soldering 10 sec / plastic package soldering 4 sec) 300 degree and 260 degree. what is the exact meaning of this temperature?
3. Here is the most important thing. the customer spec. is 12V input and 8V output, maximum output current is 3A.
is it okay to use LM350A under this condition? (I think it is pretty negative, because of junction temperature and power dissipation.)
if it is not okay, could you recommend other way to reduce switching noise for this customer spec.? I think 2 stage LDO circuit is okay, just if not use DCDC.
please check these issues. Thanks.
Best regards,
Chase