Hi Team,
There is a good new we that DIN TPS2HB50BQPWPRQ1
I want to ask about the setting of TPS2HB50BQPWPRQ1,
please refer to the Table diagram in the figure below
1. What is SNS output High-Z? Is it high impedance?
2. Which pin of the IC does FAULT DETECT refer to?
3. If you want to measure the Current of CH1 & CH2, is it the only way to switch between them?
Set it to 1000 for a short time and 1010 for a short time, and then set the current, only the current of the current Channel will be displayed on the SNS pin?
4. If the function is to monitor the load current, is it set to 1000 and 1010?