This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO5451: RST reset pull up resistor value

Part Number: ISO5451


Dear Teams,

My customer is asking what is the resistor value on the internal RST pin? The reason they are asking is because they have a reset signal with maximum output current capability 50mA. They are wondering whether it can successfully apply a low pulse to reset the fault latch?

Thanks!

Dylan