Hi,
I'm having difficulties in understanding how the Pro interface for bq Evaluation Software 0.9.92 works.
The test condition require an input to ManufacturerAccess() 0x0022 – FET Control and to read back the output from SMB Register ManufacturingStatus() which is expected to be 0x0168 (Bit 4 - FET Flag
Cleared) and also from SMB Register OperationStatus() which is expected to be 0x00106101 (Bit 2 - CHG Flag Cleared; Bit 1 - DSG Flag Cleared).
May I know how the input will be written in the bq Evaluation Software 0.9.92 and how i can read back the result from SMB Register ManufacturingStatus() & SMB Register OperationStatus().
Thanks