Hi team,
our customer used multimeter to test the ILIMIT pin voltage of multiple chips (sample number 30), and found that there is a big difference with the current given by the research and development.
Test method: using multimeter test ILIMIT pin voltage
The Rlimit resistor they use is 39k. According to the current of 10.5uA-11.5uA, the corresponding voltage range is 409.5mV-448.5mV, but they actually tested multiple chips and found that under normal temperature all devices will be lower than the lower limit as datasheet gave 409.5mV, the statistical results are shown in the figure below.
Test Results: MAX=408mV; MIN=360mV; AVG=378mV.
caculated TYP=436.8mV
1. According to the data you researched and developed (Ilim current 11.2uA, Rds(on) resistance 0.68mohm), the calculated over-current protection typical value is 36.763A
2. According to our statistics, the average value of Ilim current is 9.7uA and the Rds(on) resistance you researched and developed is 0.68mohm. The calculated overcurrent protection is typically 31.389A.
3. According to our statistics of the Ilim current average value of 9.7uA, the Rds(on) resistance in your specifications is 0.58mohm, the calculated over-current protection typical value is 37.385A
In view of the fact that Ilim current and Rds(on) resistance have a great influence on the overcurrent protection point, please help to reconfirm the typical values of Ilim current and Rds(on) resistance at room temperature. If it is convenient, please help provide Ilim current and Rds(on) ) Distribution diagram of resistance