Hello,
I had a couple of questions regarding the TPS24720.
How does one find the relationship between the current through the sense resistor and the voltage at the IMON pin? The datasheet simply says that they are proportional but what is the constant of proportionality? Will the voltage at this pin be affected by the current limit I set? A graph or an equation for calculating the IMON voltage would be helpful.
And in the design calculator the input cells for the capacitance values specify that it should be given in nF. However when looking at the design summary the same numbers are taken but given in uF without any factor of 1000 conversion. What is the correct unit for these capacitances?
Martin