Other Parts Discussed in Thread: LM5156
Hi Team,
Our customer wants to design a power supply using LM34966 with the following specifications.
Minimum input voltage = 8V
Maximum input voltage = 24V
Output voltage = 150V
Power Output = 80W
Upon simulating the device with Webench it seems that this is not possible using LM34966 and the solutions provided are using flyblack converter. However, our customer would like to use the voltage doubler as shown below. The output from the boost converter is 40V, 2.5A. Is this possible? If yes, can you please suggest one that would work for this application?
Regards,
Danilo