Stuck on the LM2577 again
I have the design bread-boarded and sort of working for 12Vin and +-15 volts out so that means I willl require the Snubber circuit as well.
as the the transformer is Lp=200 and the input voltage is 12 and the max I is 300ma
Now I am stuck on how Ip(PK) is derived?
Was using a '1N4148' in the circuit as the FRD so far I have been just plugging in values
.33 uf for C and 250 ohm for 'R' seem to work but are these even close?
I can't seem to figure this one out.
Cheers
John