Hello TI experts,
My customer considers LM73100 for their new product, they just drew 1st schematic.
as same as the schematic, they will use 2 LM73100.
the point is, 2 outputs are tied together. and each output have a possibility of different voltage.
because first IC's input would be fixed 4.3V, but second IC's input is the battery. it will change to minimum 3.6V.
they thought for this circuit because 4.3V is main power, also use battery for backup.
could you check this tied output, different voltage is okay?
also please let me know if there any points to change in this schematic, like RLC or something. Thanks.
Best regards,
Chase