This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi all,
I have designed power supply using LMR36520, but due to unavailability i have chosen LMR33620 which is pin compatible. I have assembled 5 boards with LMR33620. When powered on the device is getting short circuited immediately on pins 1(GND), 2(VIN) and 8(SW).
I have verified design with WEB BENCH tool and I have not find any design issues.
Please suggest why this device is getting damaged.
Design specification
VIN - 24VDC, 2A through a certified adaptor and adaptor output cable length is 1Foot
VOUT - 5V 1.5A

Hello
The input EMI filter may be causing an overvoltage on the input.
The ceramic input capacitors have very low ESR, and will ring with the EMI filter L.
Try connecting a 22uF or 47uF Al. electrolytic capacitor across the input of the device,
as an experiment. The ESR of the Al capacitor will provide damping to the filter.
Also, please provide PDFs of your PCB layout for us to review.
Keep in mind that the LMR33620 is only rated to 36V
Thanks
Dear Frank De Stasi,
Actually we have given provision for EMI filter in the design, while testing the proto PCB we have not populated the inductor L1 (shorted pads with thick wire ) of EMI filter, remaining all input capacitors are mounted. Note that C1,C2,C4 & C5 are AL.Electrolytic and only C6 is a ceramic cap.
Using bulk caps like 22uF or 47uF can create high inrush current. Moreover WEB BENCH tool did not suggest to use bulk caps on input side. And doing multiple experiments is not possible because of shortage of samples and high lead time. So please try to give an exact solution.
I will send PCB layout file in a while.
Hello
Please also send waveforms of the voltage on the VIN pin and the SW pin of the device during you testing.
Thanks
Hello Frank,
We have tested the board by adding 47uF AL-EL cap on the input side of the regulator and observed the following waveforms on VIN pin and CBOOT pin. Channel 1 is input supply at power connector. Channel 2 is VIN(2) pin of regulator. Channel 3 is CBOOT pin(7) of regulator. Unfortunately we have not measured SW pin, at the time of power on.

This time device is not getting short circuited but the device is not generating the output voltage. Observed a 5V at CBOOT pin.
Channel 1 is input supply at power connector. Channel 2 is VIN(2) pin of regulator. Channel 3 is CBOOT pin(7) of regulator.

SW pin is measured 500mV as shown below. Output is also 500mV instead of 5V.

Hello
It looks like you have some very bad waveforms at the input to the regulator.
You should test with a stable bench supply and see if you get better results.
That would be the best starting point to troubleshoot this issue.
We also need to see your PCB layout to help further.
Thanks
Hello
The component designators do not correspond between the schematic and your layout.
Please provide a schematic that has designators that correspond to your layout silk screen.
Thanks
Hello
I am assuming that the area of the LMR33620 is as shown in my attachment below
Here are my comments
1. The 220nF input capacitor must be on the same side as the device and close to the VIN and PGND pins
2. A 4.7uF or 10uF ceramic input capacitor should also be used and placed next to the 220nF. The Al electrolytic can be retained if desired, in addition to the ceramic.
3. You need vias under the DAP of the device to connect the ground planes for good thermal and electrical performance.
4. Be sure that the feedback divider is close to the device and grounded near the device
5. Try to achieve a better ground route for the VCC capacitor.
6. You need some ceramic capacitance on the output. See data sheet for recommendation. You can retain the Al electrolytic if desired in addition to the ceramics. The output capacitors should be grounded near the ground of the device. See data sheet.
7. Please see the PCB layout example in the data sheet for details regarding the above comments.
Thanks

Sir, we have the same problem. I try to replace LMR36510 with LMR33620, but get burned.
But it simply worked after I removed the one of Enable resistor which connected to gnd (in case on your schematic: R139 and R140)
Worth to try.
Good luck
https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/1010097/lmr33620-alternate-of-lmr36510-but-get-hot-burn?tisearch=e2e-sitesearch&keymatch=lmr33620#
Hello Frank,
Thank you for reviewing the PCB layout.
1. Vias under the DAP of the device to connect the ground plane, are already there in the layout. They are not highlighted in the pdf attached.
2. You are suggesting to add extra ceramic cap on both input and output side of device. Refer to your comment on jul 7, there you have mentioned that usage of ceramic caps will lead to ringing. So why it is not considered here.
3. I accept that, changing the layout according to your suggestions may increase the device performance, but I don't think device will get damaged with those reasons.
4. All 5 boards that I have made assembled, got damaged. I have replaced new device in one board and tested with 10uF Ceramic on input side and output side also, even though device got damaged.
5. I have used different buck converters from TI, but never faced any issue like this. I have seen others posting the same issue in the forum.
No one got the correct solution.
Hi Khyarui Arham,
I have seen your post earlier and given a try removing the resistor. But it did not help me.
Hello
Did you try placing the 220nF and 10uF close to the device VIN and GND pins?
Also, did you try with an external supply?
Thanks
Hello Frank,
Yes I have placed 220nF closed to Pin 1&2 of the LMR33620 and also placed 10uF cap. Changed input power source.Even tough facing the same problem.
Desoldering from one board and soldering it again in another board is also causing the damage to device without switching the power ON.
Procured 12 devices totally, out of them 10 got damaged during all these exercises. I am really disappointed with this device.
Thanks
Hello
Have you tried using an external clean input supply connected to your board?
Thanks
Hello Frank,
Yes our LAB supply is certified and working fine and clean regulated output. We are using lab supply from Scientific and Adapter we used before is from Sony .
Thanks
Hello
Did you see an issue when connecting the lab supply directly to the input of the regulator ?
Thanks
Hello Frank,
Yes I have seen the issue using the lab supply. Tried two ways, one is hot plugging and the other is switching on after connecting the supply. In both cases device got damaged.
Thanks
Hello
I still believe that it is some kind of overvoltage event or severe noise on the input.
Can you take a scope shot of the input voltage when you are using the bench supply.
Also, what load are you using during the test?
Thanks
Hello Frank De Stasi,
I could not give reply because I am out of station these days. The issue is not solved yet. I did not see any over voltage event with my supply. I used the same supply for another board which contains TPS54302 regulator from TI and it is working fine. Find the captured images of bench supply output voltage. It is clean, no over voltage and a ripple of 540mVp-p. Load on the device during test is 1.5A maximum. I believe that only LMR33620 is creating some issue when powered with this supply.


Hello Sreehari,
I am of a similar opinion to Frank.
From your layout I observe that the path from +Ve input terminal of the board to the VIN pin of the device must travel from the top side of the board, down to the Layer 8, and back up to the top side of the board. This is a large input loop which will result in larger than necessary parasitic inductance which will result in ringing on the input node. This ringing may be exceeding the absolute maximum voltage rating for the input pin which is resulting in the device being damaged.
Could you please take a scope shot of the input voltage when using the bench supply when turning on the device?
Ideally what I am looking for in the scope photo is as follows: Input voltage at the pin of the LMR33630 device, the SW node voltage, and the input supply at the power connector.
Regards,
Harrison Overturf
I just read again the difference between LMR36510 and LMR33610 is LMR36510 has internal soft-start circuit, but LMR33610 doesn't. In other side I have much MLCC to filter the input power, so it may cause the big inrush-current problem. You should add a soft-start circuit. It works on me:

You can calculate the voltage divider: R1 and R2 based on Vg threshold of the Mosfet. In my case I have input voltage range from 9V to 36V. To add more time/delay on soft-start circuit you can change the C1 value bigger than 1uF (I use 10uF/25V MLCC)
Hi Khyarul,
Thanks for your reply. This is an innovative solution.
Just to clarify however that both LMR33610 and LMR36510 have internal soft start circuits with nearly identical soft start times.
Regards,
Harrison Overturf
Oh I didn't found it on the short description of LMR336xx, may be I missed it. Thanks for the information...