Other Parts Discussed in Thread: TPS53819, TPS53819A, CSD86350Q5D
Hallo,
We are using the CSD86360Q5D in our DCDC converters together with the TPS5381A.
I have already successfully simulated the circuit with TinaTI, but now I wanted the a Simulate the whole with PSpice, because there are better applications here. Unfortunately, a simulation is not possible with the exact same circuit diagram. The result does not correspond to the actual processes.
There is an example circuit for the TPS53819 which is working as expected so I suspect that this is not the problem.
So would it be possible to check the model for the CSD86360Q5D?
Thanks!