This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
This question is intended for both TPS544B20 and TPS544C20.
The device has to be mounted on PCB while writing the NVM. The input 12 V is supplied, the device is turned on, and the output is enabled.
Best regards,
Shinichi Yokota
Hello Shinichi,
Per the datasheet's description of the STORE_USER_ALL (15h) command. It is permissible to write to NVM during the device's operation. Please note that the device will continue operating and ignore the fault conditions until the memory write is complete (this process may take on the order of ms). So long as the device does not experience any faults that could damage the device during an NVM write such as a short circuit event or the like, this is permissible. Other than the device ignoring the fault response during an NVM write, this will not have any negative impact on the device operation in terms of regulation.
Regards,
Alec Biesterfeld
Alec,
I'd like to ask some additional questions.
Best regards,
Shinichi Yokota
Hi Shinichi,
There is not a specified limit to the number of NVM write cycles for this part.
If using the BPEXT function, the BPEXT pin must be powered at a minimum in order to write to NVM and use the PMBus interface. Otherwise, the VDD pin must be powered if you are not using the BPEXT option to store to NVM and access the PMBus interface.
Regards,
Alec Biesterfeld