Hi,
I am trying to run the LM25011 PSpice Transient Model from the product page (https://www.ti.com/product/LM25011#design-development) with PSpice for TI (PSpice_TI 17.4-2020 S006 Windows SPB 64-bit Edition) on Windows 10 Pro. The simulation fails and does not produce any usable output at all. I am very new to PSpice so it could be just me using the software wrong. What I tried so far:
When opening the project a message pops up:
"INFO(ORCAP-2459): TI model librariers have been updated to the lates version in this design. Refer to the session logs for details of these updates."
And then a message that it is a read-only file:
"WARNING(ORCAP-1682): File is read only or in use. Changes will not be saved back to the original file named <path to my folder>\snvm168\LM25011_TRAN.opj"
I can the open for example the "STARTUP_TRAN" schematic and no simulation profile is selected. By selecting the "STARTUP_TRAN-STARTUP" simulation profile the PSpice asks me to save the project under a new name which I tried but at the end of the process it says that the read-only file can not be saved. The schematic closes and I can open it again this time with the selected simulation profile.
After pressing the play button it simulates forever (there is also no percentage of how much it has finished visible) and I manually stopped the simulation at TIME=0.14 which opens up the PSpice Runtime Settings:
Output of the simulation:
**** 07/08/21 15:55:56 ******* PSpice 17.4.0 (Nov 2018) ******* ID# 0 ********
** Profile: "STARTUP_TRAN-STARTUP_TRAN" [ <path to folder>\snvm168\lm25011_tran-pspicefiles\startup_tran\startup_tran.sim ]
**** CIRCUIT DESCRIPTION
******************************************************************************
** Creating circuit file "STARTUP_TRAN.cir"
** WARNING: THIS AUTOMATICALLY GENERATED FILE MAY BE OVERWRITTEN BY SUBSEQUENT SIMULATIONS
*Libraries:
* Profile Libraries :
* Local Libraries :
.LIB "../../../lm25011_trans.lib"
* From [PSPICE NETLIST] section of C:\cds_spb_home\cdssetup\OrCAD_PSpiceTIPSpice_Install\17.4.0\PSpice.ini file:
.lib "nom_pspti.lib"
.lib "nom.lib"
*Analysis directives:
.TRAN 0 3ms 0 0.1u
.OPTIONS ADVCONV
.OPTIONS FILEMODELSEARCH
.OPTIONS ABSTOL= 1e-8
.OPTIONS GMIN= 1.0E-11
.OPTIONS ITL1= 500
.OPTIONS ITL2= 1000
.OPTIONS ITL4= 2000
.OPTIONS RELTOL= 0.005
.OPTIONS VNTOL= 1e-5
.PROBE64 V(alias(*)) I(alias(*))
.INC "..\STARTUP_TRAN.net"
**** INCLUDING STARTUP_TRAN.net ****
* source LM25011_TRAN
X_D1 N16825155 SW CMSH3_60M
X_C6 OUT 0 MY_COUT_STARTUP
R_R2 FB OUT 9.76k TC=0,0
R_R3 0 FB 10k TC=0,0
R_R6 N16825155 0 0.0799 TC=0,0
R_Rout OUT 0 3.33333 TC=0,0
X_U1 VIN RT PGD SS 0 FB 0 N16825155 SW N16825119 LM25011_TRANS
C_C2 0 VIN 1u IC=0 TC=0,0
R_R1 VIN RT 147k TC=0,0
V_Vbatt N16833908 0 5Vdc
R_R4 N16833908 PGD 10k TC=0,0
C_C3 0 SS 10n IC=0 TC=0,0
R_Resr1 N16834023 VIN 10m TC=0,0
V_Vin1 N16834023 0
+PWL 0 0 100u 0 110u 13
C_C4 SW N16825119 0.1u IC=0 TC=0,0
X_L1 OUT SW LDCR PARAMS: L=10U IC=0 DCR=0.06
X_C1 VIN 0 Cin PARAMS: C_CAP=2U ESR=0.0055 IC=0
**** RESUMING STARTUP_TRAN.cir ****
.END
WARNING(ORPSIM-16534): Using high values of ITL4 for Speed Level > 0 may increase total simulation job time.
Starting pseudo-transient algorithm.
INFO(ORPSIM-16594): To improve Pseudotransient Convergence and Performance, set following options to relax stabilization criteria for capacitor currents and inductor voltages: PTRANABSTOL=1e-5, PTRANVNTOL=1e-4
ERROR -- Convergence problem in transient bias point calculation
Last node voltages tried were:
NODE VOLTAGE NODE VOLTAGE NODE VOLTAGE NODE VOLTAGE
( FB)-14.42E-09 ( RT)-160.8E-12 ( SS) 4.6821 ( SW) 11.93E-06
( OUT)-28.50E-09 ( PGD) 4.5455 ( VIN)-160.8E-12 (X_C1.3)-69.56E-12
(X_C6.1) 1.210E-09 (X_C6.3)-28.75E-09 (X_C6.5) 1.192E-09 (X_C6.7)-19.87E-09
(X_L1.3)-25.67E-09 (X_U1.1) 0.0000 (X_U1.2) 3.5000 (X_U1.3) 0.0000
(X_U1.8) 545.1E-06 (X_C6.10)-24.66E-09 (X_C6.13)-25.31E-09
(X_C6.26) 2.374E-06 (X_C6.28) 15.61E-06
(X_C6.29) 2.439E-06 (X_U1.12) -5.0000
(X_U1.14)-109.5E-06 (X_U1.20) 3.5000
(X_U1.21) 4.7000 (X_U1.22) 0.0000
(X_U1.24) 0.0000 (X_U1.27) -.1500
(X_U1.28)-80.38E-12 (X_U1.37) 5.0000
(X_U1.38) 5.0510 (X_U1.40)-910.5E-21
(X_U1.44) 1.6667 (X_U1.45) 4.0554
(X_U1.47) 3.5000 (X_U1.48) 14.55E-12
(X_U1.49) .3000 (X_U1.50) 3.5000
(X_U1.52)-160.8E-12 (X_U1.53) 5.0000
(X_U1.54) 3.5000 (X_U1.58) 0.0000
(X_U1.66) 0.0000 (X_U1.68) 0.0000
(X_U1.69) 0.0000 (X_U1.76) 2.027E-09
(X_U1.81) 2.5100 (X_U1.CL) 0.0000
(X_U1.EN)-1.390E-12 (X_U1.LO) .3000
(X_U1.PG) 0.0000 (X_U1.QN) 1.2469
(X_U1.108) 5.6943 (X_U1.ONT) 0.0000
(X_U1.REF) 2.5100 (X_U1.UFD) 11.99E-06
(N16825119) 5.7115 (N16825155)-1.481E-09
(N16833908) 5.0000 (N16834023) 0.0000
(X_U1.DC5V) 5.0000 (X_U1.ENON) 1.6667
(X_U1.EOND) 1.6667 (X_U1.FCIC) 1.548E-09
(X_U1.OFFT) 0.0000 (X_U1.REF1) 2.5100
(X_U1.UVLO) 0.0000 (X_U1.UVRC) 1.6667
(X_U1.VSDN) 0.0000 (X_U1.X3.3)-160.8E-12
(X_U1.X3.6) 548.3E-06 (X_U1.X4.4) 3.5000
(X_U1.X7.5) 3.5000 (X_U1.DRIVE) 1.2448
(X_U1.VREFI) 2.5100 (X_U1.X64.4) .3000
(X_U1.X65.4) 3.5000 (X_U1.X67.3) .3000
(X_U1.X68.3) 3.5000 (X_U1.X69.4) 0.0000
(X_U1.X69.5) 0.0000 (X_U1.X71.4) 3.5000
(X_U1.XCL.4) 0.0000 (X_U1.XCL.5) 0.0000
(X_U1.XFB.4) 5.0000 (X_U1.XFB.5) 0.0000
(X_U1.DRVNOT) 1.2469 (X_U1.QLATCH) 1.2448
(X_U1.XOFF.4) 0.0000 (X_U1.XOFF.5) 0.0000
(X_U1.XUVD.5) 0.0000 (X_U1.XUVD.6) 0.0000
(X_U1.X6.X1.4) 1.2469 (X_U1.X6.X2.4) 1.2448
(X_U1.X22.X1.4) 1.2448 (X_U1.X22.X2.4) 1.2469
**** Interrupt ****
I press "OK& Resume Simulation" and a couple of messages pop up.
First message:
"There are no data values in section number 1 Ignoring this section"
Second message:
"There are no data values in section number 2 Ignoring this section"
Third message:
"Analysis failed on <path to my folder>\snvm168\lm25011_tran-PSpiceFiles\STARTUP_TRAN\STARTUP_TRAN\STARTUP_TRAN.dat"
The same behavior also occurs with the other schematics: LINE_TRAN, LOAD_TRAN, STEADYSTATE_TRAN.
What am I doing wrong or is there something wrong with the project?
Edit: Sorry for the long post, I tried to put the simulation output in a Code environment but it keeps telling me, that I am not allowed to do so.
Access denied
You don't have permission to access "">e2e.ti.com/.../configure on this server.
Reference #18.8fd6dd58.1625753172.b72227