This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24721C: Differences case between AC adapter detect comparator (ACDET) in practice and datasheet

Part Number: BQ24721C


Dear TI Engineer,

I have an output voltage of 18V and when the voltage drops to 15.1V(VACDET<=1.2V)the BQ24721 determines that the AC adapter voltage is unstable and switches off the ACFET via ACDRV within 1us.

Of course, adding a slow ON capacitor to the ACDRV would be another case.

This is also mentioned in the Datasheet, see the marked pictures below:

However, in practice I found that the time marked in the Datasheet for the AC adapter not detected deglitch time does not match the time I actually used. 

My question is: When I break the connection between the ACDRV and the MOSFET´s gate, what is the actual enable time of the ACDRV?
I measured it to be much greater than 1 microsecond and up to millisecond. Is the Datasheet incorrectly, or is there some mistake in the way I am testing?

Please feel free to ask any questions if you are not understand or not clear.