This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCD9081: Lower I2C Speed than 100kHz

Part Number: UCD9081

Is there a way to set UCD9081 I2C speed at 62.5kHz?

It seems like the default options are 100kHz and 400kHz.