Other Parts Discussed in Thread: LMR36510, LMR33610, LM3489, TPS64200, LM3475
We are using the TPS54040 in an application which requires operation at 100% duty-cycle with very light load for up to 50ms at a time. Using the recommended boot capacitor value of 0.1uF, we cannot achieve this - the boot capacitor voltage falls below the 2.1V UVLO threshold and the internal FET turns off. The low load current is insufficient to pull the switching node down and re-charge the capacitor.
We have achieved success by increasing the boot capacitor to 2.2uF - measured on the bench, this maintains sufficient voltage to keep the FET on for the required 50ms. Are there any potential caveats to be aware of when using such a high-value boot capacitor? Could this cause problems with the internal boot-charging circuit?