Part Number: TPS7A47
Hi
Let me ask you a basic question about the output current as below.
The specification of the max current is defined as "1A" on the datasheet.
I think that "1A" is not changed by the output voltage, for example, 1.4Vout(min)/1A, 34V(max)/1A...
But there is a large difference about "power" (1.4W vs 34W).
I suppose, from "power" point of view, as the device has an ability to supply 34W, output current will be up to 24A when output is 1.4V...
Is my idea correct??
Or if we need a large power for output, we should set the output voltage as large as possible?
Thank you for your support.
Best Regards,