This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM51551: Discontinuous outputs

Part Number: LM51551

Hi, 

I am using LM51551 in my project application. Please find the schematic below. When I am applying VBATT=20V at 1V/30ms, I see that the outputs are discontinuous as shown. I have connected 80mA load at P8V output and 430mA load at P15V. Why is this behavior observed?

Thank you,

Anne