Part Number: LMQ61460-Q1
Other Parts Discussed in Thread: TPS2660, LMQ61460
Hello Guys,
Good day.
Our customer is working on a low EMI medical device. They would like to use the LMQ61460 as their DCDC regulator for 24V down to 5V and the TPS2660 to provide input protection for both reverse polarity and inrush. They would like to include an EMI filter on the input to reduce emissions. They would like to know what the recommended location for the EMI filter would be for best performance. They are deciding if it should be before or after the TPS2660.
I found from this application note that for best performance it should be after the TPS2660:
Thanks and regards,
Art