hello
I designed a power board and the attatched is my schematic. the problem is ,When no-load, the power consumption is also very large, and the inductor heats seriously.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hello
I designed a power board and the attatched is my schematic. the problem is ,When no-load, the power consumption is also very large, and the inductor heats seriously.
Hello Xiao,
Please send a completed LM5143-Q1 quickstart calculator for this design so we can review component losses.
These are 1.4mOhm FETs with high Qg (30nC at 5V). Based on the 28V to 5V conversion (relatively low duty cycle), choose a higher Rdson FET with lower Qg to reduce switching losses.
Recommendation is to set all gate resistors to 0 Ohms. Boot caps can be 0.1-0.22uF and VDDA cap should be 1uF (10uF is high for that).
Regards,
Tim
Looks like a stability problem. Please check your compensation values using the quickstart calculator (use the correct ESR for the output electrolytic caps).
Regards,
Tim