Part Number: TPS92641EVM
Other Parts Discussed in Thread: TPS92640
Dear TI-support,
I'm in the process of evaluating the TPS92640 for an application.
In the EVM I've changed Rsense to 333 mOhm and R6 to 47 K to make V_IADJ 2.5 V for an nominal output current of 750 mA.
In my testing I noticed that the ratio between the voltage across the sense resistor and V_IADJ is not 10 and not constant over the analog dimming range.
Here are some measured voltages, measured directly on the IC Pins:
V_CS = 251 mV
V_IADJ = 2.428 V
Ratio: 9.64
V_CS = 38.75 mV
V_IADJ = 330.5 mV
Ratio: 8.53
Best regards,
Martin