This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5030: Alternate Part number to LM5030 for the required Input voltage range 8.5 VDC to 15VDC

Part Number: LM5030
Other Parts Discussed in Thread: TIDA-01352, , TIDA-01592, LM3481, LM3524D, LM3488, TIDA-010057, LM25037, SG3524

I have referred following documents so please find my query/comments as under.

TIDA-01352 >> This board is based on LM5030 with push pull topology so noise is very low. It is good design but in my application I am going to operate on 10.8 V Li-Ion battery so Input voltage range is 9-15 Volt but in the TIDA-01352 board LM5030 is used so which will not work on 9-15Vdc. Still if I want to use it then I need to add boost converter and generate 24V from input voltage 9-15 VDC but it will increase one stage so i need to consider efficiency, size, cost so please suggest alternate solution.

TIDA-01592 >> This board is based on LM3481 Flyback topology. I have concern related to noise compare to Push Pull topology so please advice on it.

TIDA-010057 >> This board is based on LM3488 SEPIC but Watt is too low. LM2524D/LM3524D >> For the push pull topology in place of LM5030, LM2524/LM3524 is also seems alternative. I am seeking expert advice considering above points.

Please provide solution of my requirement Vin 8.5 to 15Vdc, Vout 0-50 (Split power supply voltage controllable 2.5 tp 50V ) watt 25 Watt or upto 10W is also but using push pull topology more or less similar to TIDA-01352.(LM5030 is not suitable due to my input voltage range is 8.5 Vin to 15 Vin)  with considering high efficiency and low noise.