HI Team,
I am not able to use webench tool as input requirements are not allowing the input voltage <14V.
Vin-5V,
Vout=3.3V
IOUTmax=1A
For TLV62569DBV, please help
Regards,
Vidhya
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI Team,
I am not able to use webench tool as input requirements are not allowing the input voltage <14V.
Vin-5V,
Vout=3.3V
IOUTmax=1A
For TLV62569DBV, please help
Regards,
Vidhya
Hi Vidhya,
We are able to create design and perform electrical simulations for TLV62569 with below inputs:
VinMin=VinMax=5V,Vout=3.3V,Iout=1A
Could you please confirm on above inputs condition?
Kindly follow the below steps to create design:
2.Enter the input conditions and click on view design TLV62569:
Regards,
Shaheen S M
H Shaheen,
when you click view design, it shows following error to change the inputs.
Please suggest.
Thanks,
Vidhya
Hi Vidya,
For above mentioned condition, Vin=2.5 to 5.5V, Vout=3.3V and Iout=2A.
As it's a Buck device, For VinMin=2.5V, Device doesn't support 3.3V Vout. Hence design is failing on WEBENCH. Please increase VinMin voltage.
Regards,
Shaheen S M