Hello,
I've been using the TPS274160EVM in order to examine the TPS274160 behavior.
1) When I shorted output number 4, and looked at the CS diagnostics pin, I expected to see 4V, according to the TPS274160 datasheet, but instead I saw 5.95V.
Did I miss something? Why the voltage was so high?
2) When I changed J5 and J6 state, in order to check other outputs CS state when there is short at the output, it didn't word.
It didn't matter which combination I put at these jumpers, the CS output gave indication only from Output 4.
What can be the problem?
Thanks,
Asaf