Hi,
I have some general design questions about this part. When attempting to chain multiple devices together by connecting one GPIO output to a second devices Monitor Input. Is there a voltage that needs to be set for "Vout" under the Rail Configuration tab for the Monitor pin that that the GPIO is connected to? Also, if a monitor pin is being used for temperature readings with an external temperature IC. What would be the Temp Cal Gain: in (Celsius/Volt). IF the output of the temperature sensor is defined as Vptat=4mV/Kelvin. The specific temperature sensor IC being used is LTC2997. Any help would be much appreciated.
Thanks,