This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC29002: UC39002 for HV application( 28V output) - Rbias1,Rbias2

Part Number: UCC29002
Other Parts Discussed in Thread: UCC39002

Hii,

i am using UCc39002 for load sharing between multiple power supplies, output voltage 30VDC,

The schematic is as per below , how to setup Rbias1 and Rbias2 for 30V application,

i am using 2.8K for Rbias1 and 2K for Rbias2