This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ2000: Recharge of 2 NiMH cells via USB port

Part Number: BQ2000


Hi,

I have to design a charger for two NiMH cells connected in series. Charging takes place via the USB port.
The questions are only the following:

1) Is the BQ2000 driver able to detect non-rechargeable alkaline batteries and then automatically suspend the charge? At the moment the only device that declares it on the datasheet is the Maxim DS2712.

2) Is there a driver for charging NiMH batteries that integrates the USB BC1.2 standard? I ask because the device I have to design, if connected to the PC, limits the charging current to 500mA, if connected to a charger it limits the current to 1A.

I hope I've been exhaustive.

Regards,
D. Facchini

  • Hello,

    1. I am confused, why would you put a non-rechargeable battery into a battery charger?

    2. Please see the attached Application Note on charging NiMH batteries. Can you please provide more details about the features that you are looking for so I can try to find a charger that can be used with the below scheme?

    https://www.ti.com/lit/an/slua843/slua843.pdf

    Thanks,

    Mike Emanuel

  • Hi,

    The apparatus that I have to design will have a compartment where it will be possible to enter both Alkaline AA battery and rechargeable NiMH batteries.
    This apparatus will have a USB Type C port to make the data connection with the PC and I would like to avoid damage if the user used Alkaline batteries.

    This automatic recognition function is fundamental for this application, there are drives who integrate it?

    Regards,

    D. Facchini

  • Hello,

    The BQ2000 does not detect if the battery is rechargeable or not. As such, you will need to design a system where only rechargeable batteries are connected to the battery charger and non-rechargeable batteries are not. Alternatively, you will have to create some circuit, logic, or user input to connect the charger to rechargeable batteries only.

    Thanks,

    Mike Emanuel

    Please click "Resolved" if this answered your question.