Other Parts Discussed in Thread: LM337
I have built two prototypes of a dual rail +-15V PSU using LM317 and LM337 devices. The circuit is attached. Both boards are suffering the same problem.
When the output rails are very lightly loaded (power indicator LEDs only, so around 15ma per rail) then the output voltages are correct at +-15V.
However when I raise the load above 100mA then the +15V output rail falls to +6.96V. It starts to fall after about a second and takes around 10secs to fall to that level, where after it remains at that level.
You will see the circuit contains a 'mutual shutdown' element which is designed to protect 5532 audio ICs from being fed from only one rail, should the other rail fail.
With that mutual shutdown circuit in place (and the output loaded above 100mA), I get the following voltage readings on the two devices:
LM317
input +6.96V
output +5.36V
adjust +4.92V
LM337
input -39.9V
output -6.08V
adjust -4.82V
I have also attached an AC coupled scope image of the +15V rail output rail.
Note the huge imbalance between the input voltages to the regs (under light output load these are the same at around 23V into each device).
I have tried removing the mutual shutdown circuit and found that it is the +15V rail which falls under load. The -15V rail remains at the correct output voltage, so it seems I have a problem with the LM317 circuit or pcb layout. I have built two of these boards so it is unlikely to be two faulty LM317s.
Your help to resolve this issue would be appreciated.
Regards
Robert