Other Parts Discussed in Thread: TPS62810-Q1, TPS62816-Q1,
HI Sir,
We followed the reference schematic of TPS54618CQRTERQ1 from WEBENCH Power Designer (please see the picture as below), but Vout looks like an abnormal rising when we measured it during power on (please see the waveform as below). Do you think the phenomenon brings any potential risks ? If yes, how to modify the circuits?
<Condition>:
Input: 5V
Ouput:1V@2.8A
Temperature: 85 degree
Switching Freq.: 1.974MHz
<Waveform>:
Vin
Vout : it has a drop and two stages rising.