Other Parts Discussed in Thread: TPS61022, TPS61021A
Hi
I am working on a project where I need to boost the voltage from a very low voltage source 0.65V (Input) to 5V 1 Amp output, The datasheet suggest the TPS61023 is having a wide input voltage range from 0.5V to 5.5V.
I am a bit unclear about the startup- voltage, It suggests a minimum 1.8V input voltage for startup, Can TPS61023 be used with the above mentioned parameters?
Regards
Pranav Dosajh