Hello, I have a design where two TPS63000 are supplied by lab power supply at 5V or a battery at 2,4V,. One of them is set to provide 5V, other is set to provide 3.3V.
While my PCBs were under test, 3 of these PCBs have TPS63000 burned, Looking at the datasheet, these components are protected from short circuit currents. At the input I don't see any possiblity of over voltage. However at the output, there are several possibile reasons which can cause disturbances, for example I have connectors for microcontroller programmers etc.
Using multimeter, I detect a short circuit at the input pins and not at the output pins. I would be grateful if you can share some insight that can help me debug my design. For example what are possible situations at the output that can damage these components.