I cannot find any mention of a minimum qualification voltage in the datasheet; does this IC have a minimum voltage for charge qualification?
For example, some battery charger ICs refuse to charge batteries that are lower than 350mV.
I suppose this is a protection so the IC does not attempt to charge old/damaged batteries or a battery that is inserted backwards
Does this chip have such a minimum voltage for charge qualification?
Also a general question about voltage thresholds...
• The OVP of 1.7V seems very high, too high to hit repeatedly in daily/regular use.
On NiMH battery datasheets, 1.7V while charging is an extreme maximum ... https://eneloop101.com/wp-content/uploads/2017/02/HR-3UTGB.pdf
• The Vrecharge is stated in the datasheet as 1.330V (1.305-1.355V), which also seems high, too high to begin a charge cycle
Measured open-circuit, I would expect the OVP to be ~1.4V and the Vrecharge to be ~1.2V
Can you explain why these voltages are so high?
Perhaps these voltages are the elevated voltages while the IC is active or in a charge cycle?
Thank you