The TI E2E™ design support forums will undergo maintenance from July 11 to July 13. If you need design support during this time, open a new support request with our customer support center.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS63806: chip over heat

Part Number: TPS63806

In three of the 50 printed circuit boards, the TPS63806 chip was abnormal. And the load of TPS63806 is very simple, with only one NB communication module. The input applied voltage is 3.6V. The chip will appear this situation, the power supply is applied but not enabled, that is, when the EN pin is low, the chip's VIN will have a current of dozens of mA. After the chip is enabled, that is, the EN pin level is raised, the current of Vin pin continues to increase. Accompanied by the obvious phenomenon of fever. The schematic diagram Figure 1 shown below is the specific environment in which TPS63806 works. Here is some screenshot in attachment..

TPS63806_overheated.docx