My customer is looking into using the TPS92630 LED driver in a scenario where, at high ambient temperatures, it is possible to operate the driver in the thermal foldback mode.
Is there any reliability or lifetime concern with operating the driver in this way, or does the protection mechanism sufficiently protect the device?
I believe this shouldn’t be an issue as long as the IC power dissipation using thermal foldback can maintain junction temperature below Tj-max spec of 150degC at max ambient temp and avoid continuous cycling into overtemperature shutdown mode - is this understanding correct? Is it sufficient to estimate the Ptotal and Tj using the equations in section 10.4.1 in the datasheet?
Thanks,
Alan