Other Parts Discussed in Thread: LM337
I am using the LM317 and LM337 on a dual rail +-15V PSU design. They are in the TO-220 package and have heatsinks attached.
I'm going to be pulling around 1A per rail. Although I believe my heatsinks should be up to the job, I want to measure the temperature on the devices to ensure I am staying well below the maximum recommended operating temperature.
I have two questions related to this:
1. Where is the correct place on the LM317/337 devices to measure the temperature? Is it on the plastic body or the top metal tab?
2. What kind of temperature measuring device is most practical to use? I am thinking of the very small surface area available on the device, especially if I have to measure the top metal tab temperature. There are plenty of low cost thermocouple based Probes e.g.
but I'm unsure whether I'll get an accurate temperature reading based on touching the probe tip to the device.
This is the first time I've attempted this type of temperature measurement, so your advice would be appreciated.
Regards
Robert