The User's Guide for this evaluation Module quotes:
"This evaluation module is designed for ease of configuration, enabling the user to evaluate many different applications on the same module."
The default configuration is set to:
- Vin = 18V to 36V
- Vout = 5V at 4A
My question is: How can we reconfigure this evaluation module for:
- Vin = 10.5V to 60V
- Vout = 12V (3A)
Thanks.