I want to configure an inverter circuit using CSD95379Q3M.
I checked the data sheet of CSD95379Q3M and decided that if the PWM signal could be input properly from the outside, one CSD95379Q3M could be used to configure a half-bridge inverter circuit, and two could be used to configure a full-bridge inverter circuit.
Is my judgment that an inverter circuit can be made using CSD95379Q3M correct?
If it is correct, are there any special precautions when using it as an inverter circuit?