Hi TI Team,
What is the meaning of date hold time?
The spec doesn't find this timing
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Please refer to I2C specification at https://www.nxp.com/docs/en/user-guide/UM10204.pdf and search for data hold time.
Thanks,
Ning.
Hi Ning,
I have two other questions
1,When BQ25619 is charging normally, short SYS to ground. At this time, there is still an input current of 190mA. Is this normal? If it is normal, what is the main consumption of this current?
2,The device will automatically resume normal operation once the input voltage drops back below the OVP threshold.Is the restored register the default register or the written register?
Hello Switch,
Are you referring to the charge current after SYS is not connected to ground? Or the input current while SYS is grounded?
It should be the same register values as before OVP besides the detection register: https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/1015633/bq25601-input-overvoltage-protection-behavior?tisearch=e2e-sitesearch&keymatch=BQ25601%20ovp#
Sincerely,
Wyatt Keller
Hello Switch,
Can you define your test further? There's not enough information to help determine any inconsistencies. Do you have a battery connected with BATFET off or on? Are you testing on an EVM or custom board?
Sincerely,
Wyatt Keller