This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61087: Compensation Design

Part Number: TPS61087

Here is the condition for boost design, and we're trying to get a better compensation values by Webench.

After running the Webench with below conditions, the suggested values are Rcomp=105K, and Ccomp=820pF. however, when using equation on the d/s to do calculation, the result is Rcomp=270K, and Ccomp=206pF

I'm a little confused which one of the calculation results is correct? 

Vin=5V

Vs=17.5V

L=6.8uH

Cout=40uF