Other Parts Discussed in Thread: ADS8332
I refer to the ads8332 datasheet to design the voltage reference circuit, but the final output voltage is 20mV more, and my design voltage is 4.096V,where R239 is 0ohm
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Chengxin,
Is your voltage reading from a simulation or from bench testing?
If it is from simulation, can you share the environment used to make the simulation and where you got the vref model?
If it was bench testing, can you give me the following voltage measurements (per the schematic):
It would be helpful to get scope shots of this, too, since you have a lot of capacitance at the output of the op amp.
-Tony
Hi Chengxin,
Thanks for providing the details for me.
I am looking into this - I will get back to you shortly.
-Tony
Hi Chengxin,
I have a feeling I know what the issue is - my guess is that the supplies of the op amp are flipped. V+ should be 5V and V- should be 0V. Can you confirm which pins are the V+ and V- and measure them?
If they are indeed flipped, reverse them (assuming the op amp is not killed) and take the measurements. You may need to replace the op amp if it was killed.
-Tony