Hi,
I have a high current ORing application. Where a set of each 3.3V,5V and 12V, PSUs are ORed and fed to backplane ( cPCI, VME etc) . The current on these PSU can range between 10A to 120A on 3.3V and 5V. For 12V, it is less than 10A. The question I have is:
1. To handle the power dissipation on FET without heatsink (only PCB pad) I want to use four FETS in parallel ( 8 for bidirectional blocking). Is TPS2413 designed to drive multiple FETs that require fast turn OFF?
2. Is there a way to use multiple TPS2413 in sync so that paralleled FETs can be controlled by individual device and high current handling setup be achieved?
Any other devices that can be used in this kind of application. It seems TPS2413 like devices are geared for board level use.
Thanks