Other Parts Discussed in Thread: BQ24232, BQ2432
Hi,
Good Day. I have a customer who is working BQ24170. Please see below his query for your reference. Thank you very much.
Hello, I want to know if it's possible to have max charge current of 90mA for a single cell 3,7V 90mAh li-po battery.
When setting up fast charge current (which is the max charge possible), per bq2417x datasheet,
I_charge = V_iset/(20 * R_sr)
V_iset minimum value for charger to work is 120mV.
So, putting in the values:
I_charge = 0.12/(20 * R_sr)
R_sr = 0.067 (67 mOhm)
However, the datasheet says that the full-scale differential voltage between SRP and SRN is 40 mV.
Now, I'm unsure what SW pin voltage is when input supply to BQ from adapter is 12V (like shown in Figure 19).
I guess it follows the input?
Anyhow, differential voltage between SRP and SRN limit throws me off. So what's the maximum current sense resistor R_sr can I use here?
I know I'd use a lower charge BQ, however, very few ICs from TI have an option to use external MOSFET (Q1 and Q2 in figure 19 in datasheet), which allows me to have 12V @ 3A at the System output.
Best Regards,
Ray Vincent