Part Number: LM76003-Q1
Hello,
I am designing a dc-dc converter with part LM76003QRNPRQ1 and after reviewing datasheet and simulator results I do not understand well input capacitors selection criteria.
According to the datasheet it is required a input capacitance for decoupling from 10uF to 22uF (taking into account dielectric and also derating capacitance).
But after I perform the simulation of my design I only see two capacitors in parallel of 4,7uF whose derating at input voltage make them to be about 2uF each.
Simulations seems to be Ok and match with the selected values according to the formulas.
I have also checked the example of the datasheet and it includes two 4,7uF in paralllel. Also the same case for the eval board in the whole input voltage range of the device.
I attach the simulation generated file for your checking and also some captures to show evidence about what I am talking about.
Although I've got experience on this and I know that a minimum input capacitance is always required, that makes me feel confused very often.
So, what is really the minimum capacitance required to be added in the input of this driver according to my design (input voltage 44V, output voltage 12V?
Regards,
Aaron