This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM25118: LM25118 Schematic

Part Number: LM25118

Hi,

We want to use the LM25118 for one of our products and for the same we made a schematic as attached.

We will be connect adapter on the input size and the adapter range is 15V to 24V , 5A and On the output side we need 15V,5A.

So Can someone help us to verify the Connection?

Thanks,

Yamini

  • Hello Yamini,

    The connections seem to be ok. I did not calculate all external components though.

    In general I would recommend some spare components, in case they are needed:
    - gate resistors
    - snubbers on the switch nodes
    - filter on the CS to CSG pins.

    Check out the EVM for the connection.

    Best regards,
    Brigitte