1. Is it a known issue that BQ78350-R1 a shutdown command that may brick the fuel gauge (cause firmware corruption)?
2. With reference to statement below, can you elaborate when will the SMBUS write to the data flash during shutdown process if we only send a shutdown command?
Reference statement: "Maybe there were SMBus writes to the data flash during the shutdown process which is a long process." [Source: e2e.ti.com/.../bq78350-r1-bq76930evm-bq78350-r1-bq76930-don-t-wake-up-on-shutdown-mode]
3. Is there a way to lengthen the shutdown process time to make sure all writes to the dataflash are completed during the shutdown when using a SHUTDOWN command?