Hi team we are using TPS7A8400A to generate 1V from 1.5V . I have attached the image which shows the connections of the regulator. I request you to review the connections.
The output capacitors are of 0805 package
--
Regards
Keerthana
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team we are using TPS7A8400A to generate 1V from 1.5V . I have attached the image which shows the connections of the regulator. I request you to review the connections.
The output capacitors are of 0805 package
--
Regards
Keerthana
Hi Keerthana,
With TPS7A8400A, the output can be generated with the ANY-OUT format:

If the feedback network is better for your application, the recommended values are as followed:

It is recommended that R1 is at least 12.4k to optimize noise and PSRR. The combination in your schematic does give Vout=1.001V, however it is worth mentioning the recommendations.
Overall, the schematic looks fine, they have followed the suggestion of capacitor size and type of 0805 ceramic capacitors, and even the 47||10||10 combination.
Lastly, I noticed the schematic says current= 3A, is this the intended load? If resistive load is used, make sure to use the correct value and wattage rating. i.e 0.333ohms and something that can withstand 3W.
Best,
Edgar Acosta
Hi Keerthana,
You are welcome, I am glad I could help. Thank you for contacting us.
Best,
Edgar Acosta