Hi,
I am trying to simulate TPS543320 based power supply design but I am constantly getting the following error:
ERROR(ORPSIM-16550): Floating point computation failed during matrix solution. Possible solutions: 1)Ensure that all device parameters are in valid range. 2)Try using .options LIMIT
Below is my circuit:
V12 1 0 12.00
Ven 5 0 PWL (0us, 0) (20us, 5) (20ms, 5)
Rvin 1 2 0.10
Rcin1 2 3 5.00m
Rfsel 6 0 8.06k
Rmode 7 0 174.00k
Rpg 9 10 10.00k
Rfbh 15 11 10.00k
Rfbl 11 0 10.00k
Rcout1 15 16 1.00m
Rcout2 15 17 1.00m
L1 14 15 1.50u
Cin1 3 0 22.00u
Cbp5 10 0 2.20u
Cfb 15 11 39.00p
Cboot 13 12 100.00n
Cout1 16 0 39.00u
Cout2 17 0 39.00u
XU1 6 0 11 2 5 9 7 10 14 13 12 0 0 2 TPS543320_TRANS
RL 15 0 1.00
* SYNC_FSEL PGND_0 FB VIN_1 EN PGOOD MODE BP5 SW_0 SW_1 BOOT AGND PGND_1 VIN_0
* 6 0 11 2 5 9 7 10 14 13 12 0 0 2
.TRAN 20ns 3ms 0ms 20ns
I can't see any obvious error so I would need some help on this. Also, which SW pin has to be connected to inductor - SW_0 or SW_1? When I started simulation for the first time I got message that .subckt name does not match .ends name. Problem was here:
.subckt D2A_CONVERTER_9Bout d0 d1 d2 d3 d4 d5 d6 d7 d8 ref PARAMS: THRESH=0.5
.ends D2A_CONVERTER_9B
I guessed that correct syntax would be:
.subckt D2A_CONVERTER_9B out d0 d1 d2 d3 d4 d5 d6 d7 d8 ref PARAMS: THRESH=0.5
.ends D2A_CONVERTER_9B
Is this right or wrong?
Regards
Goran